Hi,
Will use TPS65070 to power L138, have read its datasheet and a few related docs s few times, but still have couples of questions not clear:
1, SYS voltage should ramp up as soon as AC or USB is applied, regardless of the state of or actions on PB_IN or POWER_ON . is this correct?
2, After applying AC or USB voltage, SYS ramps up, DCDCx and LDOx are in disabled state, turning on them happens only after setting POWER_ON high(PB_IN is idle, high by default)?
3, When a battery is the only power source(its voltage is higher enough to power the system), to turn on the system, PB_IN should be low and set POWER_ON high while PB_IN is low. So the power-up triggering mechanism is different when system is power by a battery only and by either AC or USB. is this correct?
4, How to put the TPS65070 in OFF state, i.e. to turn off all the DCDCx and LDOx? Just by making POWER_ON low, regardless of the power sources(AC, or USB, or battery)?
5, In article, Powering Freon with TPS65070(slva371s), EN_DCDC2 and EN_DCDC3 are tied to GND, according to the tables in TPS65070 datasheet on page 54, if the pins are tied to "0", the relevant DCDCx will be permanently disabled. Do i still miss something?
6, What it the DCDC_SQx and LDO_SQx settings for the article in question 5?
7, In TPS65070 datasheet, some EEPROM bits are mentioned, how many of them are in the chip and more importantly how many of the registers settings are non-volatile?
Thanks,
clliu