This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55330: TPS5530

Part Number: TPS55330

I am using the TPS5530 device to create a 22V power rail to supply 1A and drive a resistive load.  Can I drive the EN input with a PWM signal at 100 Hz and 50% duty cycle to drop the effective output power to half?  Will the part handle this modulation on the enable line OK?