Other Parts Discussed in Thread: PMP9175
Hi
Our customer is considering PoE design using TPS23753A for camera application.
They already have been used to TPS23753A, so they chose it.
The output 4V/1.2A is required and the target efficiency is over 90%.
PMP8896 reference design seems to be good but this board is not purchasable for evaluation.
So I have the following question.
1.
TPS23753AEVM-235 seems to be the same as PMP8896 reference design.
Is it reasonable to use TPS23753AEVM-235 as the way of evaluation for customer requirement?
Do you have any other solution using TPS23753A?
2.
If TPS23753AEVM-235 is good choice, we want to refer it for customer's design too.
This EVM has synchronous flyback topology to achieve high-efficiency.
So we think it is important specially to design the following part of circuit (selection of D9, D10, D11 and FET)
We could refer layout guidelines on the user guide.
Could you please tell us other point to be considered to design high efficient circuit if you can share?
(For example, Tips on BOM selection, and so on)
BestRegards