This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC5955: what's the minimum GSLCK for TLC5955 that's required ?

Part Number: TLC5955

Hi Team,

I have customer that would like to use TLC5955 for panel local dimming.

And they would like to use the MCU to output the PWM as reference GSCLK, is it OK, or external crystal required ?

And, for the MCU, the max PWM frequency could only be 20M. What's the min GSLCK that TLC5955 requires ? I only see one 33MHz max in spec.

Thanks.

  • Hi, Rocson,

    GSCLK has maximum limitation but no minimum limitation.

    20M is also OK but GSCLK impacts the refresh rate.

    If you have more information and questions, you can send me emails: kenneth-du@ti.com.

    Thanks.
    Regards,
    Kenneth