Other Parts Discussed in Thread: TPS53647
Our customer is thinking to use TPS53667 and CSD95490 with the following condition.
Could you measure TPS53667+CSD95490 performance data?
We would like to know Thermal data, efficiency, load transient(25A to 100A, 40A/us).
Output voltage target is ripple is 6mV, transient is 0.6V+/-5%.
Vin: 12V
Vout: 0.6V
Iout: 120A
Fsw: 500kHz
5 phase
Best Regards,
Kohei Sasaki