Hi
I need to design a circuit which can provide 8 isolated supply rails around 12 volt for isolated gate drives. 0.25W is max power needed for each output and so total power is 2W. Obviously a simple design solution can be two separate flybuck converter that each includes: one flybuck controller and one transformer with 4 isolated outputs. This way I can have 8 isolated outputs. However, due to the cost and size constrains I’m looking for a design with only one controller. I have also small dual output coupled inductors available. Design solution shown in below uses coupled inductors . In this picture as shown only one controller is used and four output LCR are effectively in parallel. Since only one feedback is available the output voltage of the first LCR filter is sensed and fed back to the controller. However, since the loads of all four LCR and secondary outputs are identical we can assume the feedback system help also to regulate the other three primary outputs.
Now I'm wondering if this solution will work for me or not? Do I have to have a feedack at all, considering the fact that the input is fixed regulated 15 volts? Maybe this system can work open loop? If you there is any alternative solutions please let me know.