This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24171: charging temp 0~40C device

Part Number: BQ24171
Other Parts Discussed in Thread: BQ24172

Hi,

In case of "BQ24171RGYR" that we are using now, we are controlling Charging Temperature in TI JEITA spec.
In the case of a new project, it is necessary to set the temperature of "0 ~ 40"
In previous experience, Charger IC supporting JEITA could not set the above temperature.

I would like to inquire whether there is a part that supports the standard charging temperature with the same specification as "BQ24171RGYR".

thanks,

TS