This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25118-Q1: stability of overall gain loop

Part Number: LM25118-Q1
Other Parts Discussed in Thread: LM25118

Hello Dears,

I'm using the LM25118 DCDC Converter, I need to verify the stability of the circuit.

As mentioned in the datasheet, the overall loop gain is the product of the modulator gain and the error amplifier gain.

this is what I have :

I need to Know , did I should measured the phase margin relatively to -180° or the 0° line?

Best Regards,

Rana