This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC39002: Power module

Part Number: UCC39002
Other Parts Discussed in Thread: UCC29002

HI Sir 

May I know which power module can work with UCC39002 

We would like to do 54V redundant application .could you kindly give a example ?

Thanks

  • Hello Kai

    The UCC39002 is a general purpose load share controller and it can work with ANY power module providing that the module has a remote sense feature. If the module has a trim up/down facility then the UCC39002 can control it too. If the module has no means to modify its output voltage then that module is not suitable for use with the UCC29002.

    You will need to find a power module which can provide a 54V output at 1/n of your total output power. Then use at least n+1 modules in a load share system.

    Take a look at the EVM for the UCC29002 to see a typical application in detail. http://www.ti.com/tool/ucc39002evm

    Regards
    Colin