Hello Sir/Madam,
I am graduate student from University of Colorado,Boulder.I am using LM723 for my student project and I was not sure where exactly should Vz (pin 9 as per connection diagram from the datasheet -Figure 1) be connected in Figure 4.
Also, I have an LED as my load which has rating of 5volts, 20mA. Would this be fine to work with in this application?
If I plan to have variable resistor varying the output voltage from 2v-7v would this work as well?
Hoping for your feedback!
Thank you and appreciate your help in advance!
Kind Regards,
Harshith Alvakonda.