This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/UCD3138: Can I use the EADC to connect CBC fuction in UCD3138 ?

Part Number: UCD3138


Tool/software: Code Composer Studio

Can I use the  EADC ( Front End 0 or Front End 1 or Front End 2 )to connect CBC fuction in UCD3138 ?

  • Each EADC contains an analog comparator that can be used to generate CBC current limit .
    The only caveat is that you cannot use that analog comparator if the EADC is in normal mode use and converting a signal to digital to a loop.
    The EADC needs to be in PCM mode to generate CBC