Hi Sir:
I want to know how to use S3 mode. And For DDR it must be used this mode? but i can not get the single SLP_S3. The DDR do not have this pin out_put. And TPS51200 have not provide this PIN.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
TPS51200 EN pin can be connected to DDR SLP_S3 pin.
If DDR does not have SLP_S3 pinout, just connect other signal to TPS51200 EN pin to turn on and off VTT voltage.
REFOUT(VREF) is on when REFIN is above 0.39V, whether EN is low or high.
Thanks
Qian