Other Parts Discussed in Thread: TPS61021A, TPS61220, TPS61291, TPS610981, TPS610985
Tool/software: WEBENCH® Design Tools
Hi
I'm considering using TLV61220 or TPS61021A in a design powered using 2 x AA alkaline batteries.
When my device is operating it will take about 20mA. When idle it would be about 20uA.
Battery life should be about one year with the operating:idle ratio I'm using.
Would either of the above devices be recommended, or any others? I'm concerned that the quiescent current into the Vout pin (17uA) could double the idle power consumption of my device.
Thanks.