This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS22962: modify operating point for Cload is shown in uF when it appear in Farad in the results. This limit the validation of the values

Part Number: TPS22962
Other Parts Discussed in Thread: TINA-TI

Tool/software: WEBENCH® Design Tools

The modify operating point section for Cload is limiting the minimum value to 0.001, but take all values as Farad instead of uF like shown.  this gives the mininum value of 1mF when trying to change the values...which is not very useful.

any update for the webench to correct this?

I have a fall time that is way too long on my system and I need to understand why and what to change.

there is also no indication what is the threshold of the fall time...it's the time to go to 50% 25% of the original Vout?

thanks