This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PWM controlled buck DC/DC



Hi,

I would like to implement a MPPT controlled DC/DC because I would like that maximum power generated with panels will be delivered into system every "moment".
Vin will be between 26 V and 35V (Vmp will be at around 31 V), Vout will be 17V and I_max(at 17V) will be about 2.5 A.
For implementing MPPT logic I need buck DC/DC switcher with possibility of driving with external PWM signal. How can find which swither from your product list supports driving with external PWM? I am a little bit confused in this moment.

Thank you,
Dejan.