After few insertions, including insertions made with various angles (+45°, -45°, 90°), the wireless power Rx block can't work.
the VAC voltage is set 9.6V.
after damage, the VAC voltage is only about 700mV
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
After few insertions, including insertions made with various angles (+45°, -45°, 90°), the wireless power Rx block can't work.
the VAC voltage is set 9.6V.
after damage, the VAC voltage is only about 700mV
The bq51025 has input over voltage protection that will protect against voltage transients that could damage device.
A typical situation that will cause a voltage transient is moved the RX coil (phone) from a position of poor coupling to a position of good coupling the input voltage will increase and Clamp1 / Clamp2 will be needed to protect the device. This could be a case where the customer is picking up the phone slowly and then drops it. The field will increase to compensate for the increasing distance then when dropped the larger field will generate a large input voltage requiring the clamp circuit.
Clamp circuit should trip when rectifier voltage reaches about 15.1V. The Clamp1 & 2 mosfets will turn on connecting capacitors to the AC lines adding load and reduce input voltage. Also during this time the RX is sending commands to TX reducing the operating voltage.
When trouble shooting this type of problem check the voltage at RECT.
Possible problems with the clamp circuit will be using small or low voltage rated clamp capacitors. Higher ESR will reduce effectiveness of the clamp circuit.
Hi Bill,
2.) What RX coil are you using for this application and is it tuned
<TONY>: customized RX coil , the parameter is L=~15.4uH@130Khz, Rs = 153mohm@130Khz, Q=81
3.) What TX is used for this test?
<TONY>: TX product is also designed by us. COIL is type A29
BRS,
TONY LIU
Hi,
attach the PCB layout file, could you please help check it?
Bill J -- I have down loaded the file
BRS,
TONY LIU