Other Parts Discussed in Thread: TPS23525
When I go through the datasheet of TPS2350PWR, I could see reverse voltage protection for the chip using small signal diode between RTN pin and Supply RTN . Since the chip is supports oring controller, I understand output 48V load is also reverse polarity protected when two -48V input is applied with reverse voltage, as input mosfet and output mosfet body diodes connected in opposite direction. Please clarify