Hi
I have been recommend to use the bq21040 as it has wide input voltage up-to 28V, which gives me some flexibility in solar panels.
As the BQ21040 will work up to 28V, i think that should be adequate as most solar panel are either 12V or 24V, anything above that then we can request user to regulate there panels to the required levels from 5V to 28V.
As the voltage increases , does this IC work like a LDO and dispense the extra power in heat?
I was originally planning to keep a separate connector for the solar cells and additional micro USB connector, but if i was to make a custom cable that allows a 12V or 24V to connect to micro USB connector, would this be an issue? The PCB will not be connected to a PC, while solar cell is attached as there will be only one connector.
Our batteries have they own protection circuit and therefore the temperature wire is not available for external use. Can the temperature feature be disabled in the BQ21040 .
The aim is to design the circuit for the worst case, what would happen if the solar input was to gradually decrease during charging phase?
Would there be any need to have any additional protection circuit?
Are 0603 caps adequate for applications or should 1206 be better to use?
The datasheet mentions that there is a thermal pad requirement, but the footprint shows it as a SOT23