Hi,
I am using UCD9090 to design a power monitor system and I introduced a re-sequence for the system, but some time all the power rail got stuck and EN_control is low. Never go to high after re-sequencing stuck.
I am sure that all the rails are below Power_GOOD_OFF threshold.
I have re-sequence for rail #7 (UV, shutdown rail 1 2 3 4 5 6 8) and rail #9 (OV, shutdown rail 1 2 3 4 5 6). Basically, UCD9090 has EN for rail# 1 2 3 4 5 6. But for monitor port is for rail# 1 2 3 4 5 6 7 8 9. rail #7 is 5.3V from POE, rail #8 is 48V from PoE. Rail #9 is a pulse for WDT, named Kill_all.
So we are monitoring few rails that UCD9090 can not control.
Do you have any idea why the re-sequence does not work in this case?
I attached the project, circuits schematic, and fault logs (it seems that when these faults (Rail #7 UV, Rail #9 OV) happen, rail 1 2 3 4 5 6 was shutdown and never re-sequence )