This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/UCD3138HSFBEVM-029: Front end 1 is work for coppe snsing ?it works in the code of UCD3138HSFBEVM ?

Part Number: UCD3138HSFBEVM-029

Tool/software: Code Composer Studio

Front End 1 is work for coppe snsing ?it works in the code of UCD3138HSFBEVM ?

what are Front End 1 functions in UCD3138HSFBEVM ?

  • Front end 1 is used for current loop control, it sense the secondary current either through copper or current shunt. When the load is higher than 36A, the EVM enters constant current mode, where the output current is maintained at about 36A. This function is implemented in UCD3138HSFBEVM.

    Regards,
    Bosheng