Other Parts Discussed in Thread: TPS92513HV, , TPS92513, TPS92515
Tool/software: WEBENCH® Design Tools
I've been trying to build an analog dimmable driver with a TPS92513HV for several days. Unfortunately without success. The driver from the Webbench Designer runs constantly with full ILed, even when connected to VAdj 0V. I want to try the TPS92515HV now. But here I'm already failing because of the input to the Webbench Designer. In contrast to the TPS92513HV, I can enter a dimmberecih here. However, I do not understand the input. Does this mean in the picture below that the dimming range is 10-40% or 40-100%?
Is it possible to build a 350mA driver wirh 5% ILed ripple and dimming from 10 to 100%?