Hello
I am looking for a gas gauge product for a LiFePo4 battery pack (24V 30AH 8S) with only the Pack+ and Pack- terminals available. It looks like BQ34Z100-G1 is the recommended option but from the datasheet it looks like this has to be integrated with the BMS and cannot be used outside the battery pack. Also I am looking for 30AH and BQ34Z100-G1 is only 29AH.
I am looking for -40 to +125'C operating temperature as well.
Are there any products to suit this requirement? Or suggest the closest possible option.