Hello Team
the following is schematic about TLV803. The question is when the reset change to low, the capacitor will discharge current from internal mosfet, does the current will damage the mos?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Xiao,
The TLV803 can sink ABS MAX of 5mA. There should only be a capacitor on the input pin. I don't see any attached schematic but the internal MOSFET will not be damaged if you follow the recommend operating conditions and follow the typical application circuit.
-Michael
Xiao,
No risk with that schematic. The output capacitors C194 and C57 are not necessary but do not cause a problem.
-Michael