Hello, I have a battery that has a design voltage of 3700mV and a design capacity of 2400 mAh. It can be charged up to 4.2V and discharged down to 3V. I would like my battery to be only charged up to 4.1V. Can I have this chip report 100% at a capacity corresponding to 4.1V? Likewise, if I would like my battery to be discharged down to 3.1V, can I get this chip to report 0% at 3.1V? Also, would this change the way I should perform the process in determining the ChemID?
Thanks,
William