Other Parts Discussed in Thread: BQSTUDIO
Hello,
Our system uses the BQ34Z100-G1 on the system board and a 2S 5000mAh LiPo battery which is not user replaceable.
During development I have used the bq34z100-G1 EVM to log the battery charge/discharge profile and this data was uploaded to the TI GPC calculator and several Chem IDs were suggested.
I have successfully programmed the best Chem ID into the EVM using bqstudio, and then ran several learning/optimisation cycles, charging at 2A and discharging at C/10 (500mA) constant current with rest periods between the charges and discharges. The Update Status register has now successfully incremented to 0x06.
So I think I have successfully learnt a battery profile? So I have generated the golden image .srec .bqfs, and .dffs files.
My question is, are these golden image files good enough to be used to configure the bq34Z100-G1 parts on our first production units? The golden image files are based on a sample of 1 battery and 1 EVM. We only need the gas gauge to give fair representation of battery capacity and not to be highly accurate on this first build (accuracy within 10% would be good)
Also, going forward, do I need to perform the learning/optimisation procedure on several batteries to get an average profile? If so then how do I do this and merge the data from each battery into one configuration file?
Finally, could you please take a look at the register settings to check that I have correctly set everything up. I have attached the GG file for review (I hope)
Thank you
Peter