Other Parts Discussed in Thread: LP8557
Hi
I want to a PWM LED driver, SPEC as below. Is there a suitable LED driver recommendation?
1, support 3 parallel 10 series, total 30 LEDs
2, one way of 3 parallel LED maximum current > 80mA (two output drives one way LED is also OK).
3, the output OVP voltage > 40V;
4, PWM dimming mode, PWM frequency need to support 75Hz
5, have enable pin
thank you.
Jerry,