This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54232: The behavior of TPS54232

Part Number: TPS54232


Hi,

We got a question from customer about TPS54232.

Could you help us?

[Question]

Regarding the behavior of TPS54232 when the adjacent pin is open-shorted,

If there are some results of evaluation on the following cases

Could you tell me what condition it will be ??

[CASE]

① When R4 in the reference circuit diagram is short-circuited and only the capacitor is connected to the COMP terminal.

② When R5 in the reference circuit diagram is short-circuited.

③ When R5 in the reference circuit diagram is opened.

④ When R6 in the reference circuit diagram is opened.

⑤ When the output voltage of R5 and R6 in the reference circuit diagram is set to a value equal to or higher than the power supply voltage.

* For example, output voltage setting 20 V or the like for power supply voltage 18 V

⑥ Shorting both R3 and C3 in the reference circuit diagram.

⑦ When both R3 and C3 in the reference circuit diagram are opened.

⑧ Shorting C2 in the reference circuit diagram.

⑨ When C2 in the reference circuit diagram is opened.

⑩ Shorting the 3 and 4 pins of the TPS54232.

⑪ Shorting the 5, 6 pin of the TPS54232.

⑫ When shorting 6, 7 pin of TPS54232.

Thanks.

Best regards.