Tool/software: WEBENCH® Design Tools
Hi experts,
Requirements for my design, 12V input, 54V/2.4A output.
Webench gave a result of 248kHz switching frequency, can you tell me more about why this 248KHz is in use? Can I use 500KHz, a little bit lower efficiency is ok for me, most of the time the current should be less than 1A in my board, while I do need a smaller area.
Thanks
Chris