This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Brick wall current limit protection

Other Parts Discussed in Thread: TPS62125, TPS62120, TPS25200, TPS2662

Hi,

Customer wants the power supply to perform the following operations.

Customer condition ;
・Vin=6~12V
・Vout=5V
・Iout=200mA

Desired operation;
・Customers want to limit current at 200 mA.
 (Do not exceed 200mA.)
・If it exceeds 200 mA, the customer wishes to lower the output voltage.
 (Image of Brick wall current limit protection operation.)
    ex,Iout=200mA→Vout=5V Iout=250mA→Vout=2~4V



Could you tell me the recommended products?

Best Regards,
Yusuke/Japan Disty