This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14030: Switching frequency in DCM mode

Guru 16770 points
Part Number: LMR14030

Hi

By setting RT, switching frequency would be set.

LMR14030 can have three operation mode, CCM, DCM and sleep.

Is Fsw changed depending on operation mode?

1.
For example,
When RT = 11.5Kohm, switching frequency is set as 2MHz. However, actual swiching frequency would be decreased if load is light in DCM?

2.
What about the situlation of sleep mode?

BestRegards