Using the TI EVM bq25703AEVM-732 board with default setup I can not get the PROCHOT to trigger when the battery is removed.
Is there a trick or special setup required to get this trigger? Maybe there is a poorly named register need to be set in order to accomplish this?
I will include the register settings I have been using with no luck.
Additionally does TI have a recommenced power up register sequence and corresponding power down register sequence?
From datasheet page 25,
The PROCHOT triggering events include:
• ICRIT: adapter peak current, as 110% of ILIM2
• INOM: adapter average current (110% of input current limit)
• IDCHG: battery discharge current
• VSYS: system voltage on VSYS
• Adapter Removal: upon adapter removal (CHRG_OK pin HIGH to LOW)
• Battery Removal: upon battery removal (CELL_BATPRESZ pin goes LOW)
• CMPOUT: Independent comparator output (CMPOUT pin HIGH to LOW)
my register settings.