This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61230: Leakage current into the Enable pin.

Part Number: TPS61230

Hello,

I am using an external open drain circuit to enable/disable the TPS61230. I am pulling the Enable pin up to 3.3V with an external 100k resistor. I am measuring about 1.5V on the enable pin. I am seeing about 18uA of leakage in order to measure 1.5V.

Can you tell me what the leakage current is typically into the enable pin?

I am thinking I need a stronger external pullup. What value of pullup do you recommend when using an external circuit to enable/disable the regulator.

Regards,

Guy