This question is on section 8.3.10.2 of the data sheet. The second paragraph states:
When LODRV pulse is shorter than 100ns, bq2477x sets OCP limit proportional to PROCHOT ICRIT setting
(ProchotOption0() bit[8]). The IDPM function is disabled (0x12[1]=0). Set InputCurrent() to a right value even
IDPM is disabled.
My question is below;
If the InputCurrent() value is set prior to charging the battery, and then at a later time the LODRV pulse is shorter than 100ns, does the InputCurrent() need to be reset?