This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5912: ABS MAX for EN and PG

Part Number: LP5912

The data sheet indicates ABS MAX for PG and EN pins as 7V, irrespective of the VIN voltage. Please verify that the PG and EN voltages can be above VIN as long as they are below 7V.

Thanks,

Mark 

  • Hi Mark,

    It is important to keep in mind that the Absolute Maximum Ratings table shows stress ratings only.  Devices are designed, tested and characterized for opperation within the Recommended Operating Conditions.  For a robust system, please ensure that 0 < Ven < Vin and 0 < Vpg < 6.5 V.

    Very Respectfully,

    Ryan