Hi,
I am looking for a prioritized power path controller similar to the LTC4418 by linear technologies.
- The circuit is given two separate and different voltage inputs, say V1 = 32 and V2 = 36.
- The circuit is to prioritize V1 if the voltage is within the set range ( 30V - 34V for example).
- If out of range, it should switch to V2 (given that V2 is within range).
- When V1 is back within range it should switch back to V1.
Circuit must be capable of withstanding 38V - 40V
Thank you for your help,
Patrick