Hi,
Please tell me about the processing of the following pins when using with 2 phase.
· VHARE, ISHARE, SYNC
Is there a problem with connecting directly?
· SS, VSEL, RSP, RSN, RT (SLAVE side)
Is the connection of these pins on the slave side floating?
· RAMP, MODE, ILIM
Is the resistance value connected to the slave side the same value as Master, is it necessary to connect each?
· PGD (SLAVE side)
Is it possible to output both power good on the slave side with the same resistance value as the Master side and the same connection?
· EN (SLAVE side)
Can I make the same connection as the Master side? Is there a need for connection?
Best Regards,
Yuto Sakai