- Is it possible to replace high-side MOSFET by a diode and directly connect DIR to AGND for boost-mode-only operation ? Provided that I don't use circuit breaker and make LM5170-Q1 skip initial fault checking by placing a 10k-ohm resistor across SYNCOUT and AGND.
- If I have Vcc = 10V, is it possible to use a mechanical switch to close the Vcc to a voltage divider that will provide 5-V signal to EN1 and EN2 pins for channels enabling ? This is to avoid using MCU.