Other Parts Discussed in Thread: BQ35100
Hi,
I am considering using a BQ27542 in a design with a long life LiSoCl2 battery. Is it necessary to use the temperature sense resistor? Will the device function without the temperature sense resistor connected? Is there perhaps an internal thermistor I can use instead of one directly mounted on the battery if we're happy with less accuracy?
Also is this device suitable for this battery chemistry or are there any problems I should know about? I notice that the maximum charge which the device can measure is 14.5Ah. Our battery is larger than this, is it just a matter of resetting the device after we near this capacity?
Thanks,
John.