Part Number: TLV62569
Hi Team,
I see TLV62569EVM is using high SRF frequency (52MHz) of inductor, can customer use 5MHz frequency inductor as attached? Kindly advise. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV62569
Hi Team,
I see TLV62569EVM is using high SRF frequency (52MHz) of inductor, can customer use 5MHz frequency inductor as attached? Kindly advise. Thanks.
Hello Johnson,
I'm happy to help you. My advice would be to always use high SRF inductors. At this link:
you can find a detailed explanation of the inductor's complete model. Anyway, below I've reported the main picture we need for the explanation of the two reasons why you should make this choice:
-We need the inductor to behave inductively at the switching frequency (1.5 MHz circa) and for the above harmonics, so that the inductor current has a triangular waveform character. An SRF of 52 MHz will ensure it until the 34th harmonics circa. An SRF of 5 MHz will make the inductor act like a resonator, enhancing the 3rd and 4th harmonics, and kill the others, which will bring to stability and losses problems.
-the higher the SRF the less the HF noise is coupled to the output, hence less conducted EMI on Vout.