Hello,
I have connected this LED controller with STM controller on I2C.
The requirment is to make LP5562 work independent of STM controller. For example, If my controller(STM) is estimating that there is no activity going to perform in next 33 seconds then STM will go in sleep mode for better battery life. Here the requiment is to blink the LED after each 8 seconds for 1 second in its 33 second of sleep mode. If I can configure LP5562 to perform such a task then I can do that exectly before going in to sleep mode and we can achive our goal.
So is it possible to configure/program LP5562 to perform above task( to blink the LED after each 8 seconds for 1 second ) ? If yes then how?
Thank you,
Rohit