This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65262-1: Unused Channel

Part Number: TPS65262-1

I'm not using BUCK3 and I require the Pgood signal. If I want to use the automatic sequencing (MODE = HIGH), how should I connect the following pins:

VIN3

BST3

LX3

FB3

EN3

If I choose not to use the automatic sequencing (MODE = LOW), how does the above change?

Regards,

  • hi Pai,
    Setup as below:
    if BUCK3 is unused, setting as below:
    Connect FB3 to COMP3;
    Connect COMP3 to GND via 10k and 1nF (series)
    EN3 floating or tie to high
    SS3 floating
    PVIN3/LX3/BST3 floating
    The PGOOD will detect BUCK1/2's operation status.

    Either MODE low or high, the setup is same.