Other Parts Discussed in Thread: GPCRA0, GPCRB, BQSTUDIO
Hi,
Chem id 414 LIFEPO4 Battery
Ran learning cycle, no errors tested SOC accuracy 1-2% which is good for my application
But....
after 4-24 hours with just the gauge current draw (Relax)
Full Charge capacity, Filtered FCC, Unfiltered FCC changes from ~2500 to 1400
and the SOC jumps to 1 % even if the cell was at 85% charge
I have been looking into this for 2 weeks now and need some help
It almost appears like there is some kind of negative value calculated.
Thanks