This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51206: VTTREF Output Cap

Part Number: TPS51206

Hello,

My customer was planning to use 0.22 uF (D / S recommended value) for the output capacitor of VTTREF, but it became unusable due to circumstances related to parts procurement.
They want to change to a different capacity (0.1uF or 1uF).

Is there an upper or lower limit for the capacity?

(My customers are worried that oscillation may occur if adding too much capacity because the VTTREF terminal is OPAMP output from the internal block diagram of TPS 51206.)

Thank you.