This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82130: TPS82130 issue

Part Number: TPS82130


Dear Sir/Madam,

I  encountered some issue on TPS82130SILR:
- I use that ic to convert 12V input voltage to 5V output voltage at 2A
- Two pcs on different boards was not able to power up properly, the output is always 0.8V
- Another two boards was initially functional, i.e. has 5V output, however, after a certain time, suddenly the voltage output become 0.8V, and it was not able to recover back to 5V output.
- Below is my design:
 

Simulation using Webench at steady state show the output is stable at 5Vdc.

Any advice?

best regards,

kpk