Other Parts Discussed in Thread: TLV61046A
Hi,
Sorry to bother, but we face some strange issue in our TPS61096A based design. We have recently got out of production few boards in which we attempt to use TPS61096A to generate stable 24V from 3.6V supplied by Li-Ion battery. Unfortunately, the voltage on the output of TPS61096A is far from 24V. Specifically, the three boards we have tested so far have on their outputs 3, 5 and 6.7 V, respectively.
The schematic of the application circuit we have is as follows:
On the output we currently have a 10uF capasitor and 1.1 MOhm resistor.
Based on few quick test of one board I observe the following voltage (using a multimeter):
1. when EN is pulled down there is about 3V on TPS61096A Vout
2. when EN is pulled up there is 6.67V on TPS61096A Vout. Vosns is also 6.67V. In the middle of the voltage divider voltage is about 0.27V. Also I have noticed that the other side of the PCB, connected to the thermal PADs via through holes, starts to heat up.
Any ideas of what is wrong with our design?