Part Number: TPS61197
Dear TI team,
It is my first design of a led driver and i would like to use the TPS61197.
I tried to calculate the inductor value.
I succed to calculate the IL(DC) = 1,947A.
(With: Vin = 24V, Vout = 92.5V, Iout=480mA)
But for the Delta_IL(P-P) i don't know which value should i have. Also i don't know some units in the formula.
I think the unit for Delta_IL_(P-P) is (A), but i am not sure.
Could you clarify which units are used ? And which Delta_IL_(P-P) should i have ?
Many thanks,
Regards.