This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: Inquiry about input capacitor in WEBENCH schematic.

Part Number: LM5022


Hi team.

My customers want to design Boost converter using the LM5022.

The condition is as follows.

Input Voltage range : 9~36V

Output voltage : 54V

Output current : 0.6A

And he want to apply input cap and output cap as MLCC.

So I simulate through WEBENCH, and send result to customer.(Refer below schematic)

My customer have some question about input capacitor value.

In WEBENCH, the input cap is displayed as approximately 100uF(98.9uF).

Customers have 4.7uF / 100V capacitors and it is difficult to apply more than 6 due to PCB size.

So, if input cap is applied 20 ~ 28uF, please check if there is no problem.