Part Number: LP5569
Other Parts Discussed in Thread: LP55231
Tool/software: Linux
Hi all,
I'm looking for linux device driver for lp5569 which supports loading of engine programs.
Looking forward to hearing your answer.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
5684.0904 lp5569_i2c_master_w_multibyte-master_code_MSP_EXP432P401R.zipHi,
We have no linux driver for LP5569, but we have demo souce code with engine loarding by MSP432, I think it will help you on the coding effort after comparing with LP55231 linux driver.
Any more support please let me know.
Thanks!
Hi Summer,
I appreciate to your comments.
Do you have a plan to implement LP5569 linux driver for customers?
Actually I wrote the driver for LP5569 by myself based on 55231 but not yet implemented engine loading logics.
(Now I'm waiting for MSP432 launch pad from a TI branches.)
One more thing, Could I get the engine program sample source codes from the blog/videos - 
Thanks.
Best Regards,
WY, Yun
Hi WY,
We didn't have the resouce of LP5569 linux driver, if you would like to share your works with us, it should be perfect.
The before attachment is souce code of the demo, I upload the src code for the easy understanding.
Any more support please let me know, thanks!
Summer
diff --git a/drivers/leds/Kconfig b/drivers/leds/Kconfig
index 7a628c6..e651933 100644
--- a/drivers/leds/Kconfig
+++ b/drivers/leds/Kconfig
@@ -243,8 +243,8 @@ config LEDS_LP3952
module will be called leds-lp3952.
config LEDS_LP55XX_COMMON
- tristate "Common Driver for TI/National LP5521/5523/55231/5562/8501"
- depends on LEDS_LP5521 || LEDS_LP5523 || LEDS_LP5562 || LEDS_LP8501
+ tristate "Common Driver for TI/National LP5521/5523/55231/5562/5569/8501"
+ depends on LEDS_LP5521 || LEDS_LP5523 || LEDS_LP5562 || LEDS_LP5569 || LEDS_LP8501
select FW_LOADER
select FW_LOADER_USER_HELPER
help
@@ -282,6 +282,16 @@ config LEDS_LP5562
Driver provides direct control via LED class and interface for
programming the engines.
+config LEDS_LP5569
+ tristate "LED Support for TI LP5569 LED driver chip"
+ depends on LEDS_CLASS && I2C
+ select LEDS_LP55XX_COMMON
+ help
+ If you say yes here you get support for TI LP5569 LED driver.
+ It is 4 channels chip with programmable engines.
+ Driver provides direct control via LED class and interface for
+ programming the engines.
+
config LEDS_LP8501
tristate "LED Support for TI LP8501 LED driver chip"
depends on LEDS_CLASS && I2C
diff --git a/drivers/leds/Makefile b/drivers/leds/Makefile
index 3965070..14f0aec 100644
--- a/drivers/leds/Makefile
+++ b/drivers/leds/Makefile
@@ -31,6 +31,7 @@ obj-$(CONFIG_LEDS_LP55XX_COMMON) += leds-lp55xx-common.o
obj-$(CONFIG_LEDS_LP5521) += leds-lp5521.o
obj-$(CONFIG_LEDS_LP5523) += leds-lp5523.o
obj-$(CONFIG_LEDS_LP5562) += leds-lp5562.o
+obj-$(CONFIG_LEDS_LP5569) += leds-lp5569.o
obj-$(CONFIG_LEDS_LP8501) += leds-lp8501.o
obj-$(CONFIG_LEDS_LP8788) += leds-lp8788.o
obj-$(CONFIG_LEDS_LP8860) += leds-lp8860.o
diff --git a/drivers/leds/leds-lp5569.c b/drivers/leds/leds-lp5569.c
new file mode 100755
index 0000000..43d450c
--- /dev/null
+++ b/drivers/leds/leds-lp5569.c
@@ -0,0 +1,995 @@
+/*
+ * lp5569.c - LP5569LED Driver
+ *
+ * Copyright (C) 2010 Nokia Corporation
+ * Copyright (C) 2012 Texas Instruments
+ *
+ * Contact: Samu Onkalo <samu.p.onkalo@nokia.com>
+ * Milo(Woogyom) Kim <milo.kim@ti.com>
+ * Woonyong, Yun <wyyun@humaxdigital.com>
+ *
+ * This program is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU General Public License
+ * version 2 as published by the Free Software Foundation.
+ *
+ * This program is distributed in the hope that it will be useful, but
+ * WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
+ * General Public License for more details.
+ *
+ * You should have received a copy of the GNU General Public License
+ * along with this program; if not, write to the Free Software
+ * Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA
+ * 02110-1301 USA
+ */
+
+#include <linux/delay.h>
+#include <linux/firmware.h>
+#include <linux/i2c.h>
+#include <linux/leds.h>
+#include <linux/module.h>
+#include <linux/mutex.h>
+#include <linux/of.h>
+#include <linux/platform_data/leds-lp55xx.h>
+#include <linux/slab.h>
+
+#include "leds-lp55xx-common.h"
+
+#define LP5569_PROGRAM_LENGTH 32 /* bytes */
+/* Memory is used like this:
+ 0x00 engine 1 program
+ 0x10 engine 2 program
+ 0x20 engine 3 program
+ 0x30 engine 1 muxing info
+ 0x40 engine 2 muxing info
+ 0x50 engine 3 muxing info
+*/
+#define LP5569_MAX_LEDS 9
+
+/* Registers */
+#define LP5569_REG_ENABLE 0x00 /*same*/
+#define LP5569_REG_OP_MODE 0x02 /*0x01*/
+#define LP5569_REG_ENABLE_LEDS_MSB 0x04
+#define LP5569_REG_ENABLE_LEDS_LSB 0x05
+#define LP5569_REG_LED_CTRL_BASE 0x07 /*0x06*/
+#define LP5569_REG_LED_PWM_BASE 0x16 /*same*/
+#define LP5569_REG_LED_CURRENT_BASE 0x22 /*0x26*/
+#define LP5569_REG_CONFIG 0x2F /*0x36*/
+#define LP5569_REG_STATUS 0x3C /*0x3A*/
+#define LP5569_REG_RESET 0x3F /*0x3D*/
+#define LP5569_REG_LED_TEST_CTRL 0x41
+#define LP5569_REG_LED_TEST_ADC 0x42
+#define LP5569_REG_MASTER_FADER_BASE 0x46 /*0x48*/
+#define LP5569_REG_CH1_PROG_START 0x4B /*0x4C*/
+#define LP5569_REG_CH2_PROG_START 0x4C /*0x4D*/
+#define LP5569_REG_CH3_PROG_START 0x4D /*0x4E*/
+#define LP5569_REG_PROG_PAGE_SEL 0x4F /*same*/
+#define LP5569_REG_PROG_MEM 0x50 /*same*/
+
+/* Bit description in registers */
+#define LP5569_ENABLE 0x40
+#define LP5569_AUTO_INC 0x40
+#define LP5569_PWR_SAVE 0x20
+#define LP5569_PWM_PWR_SAVE 0x04
+#define LP5569_CP_AUTO 0x18
+#define LP5569_AUTO_CLK 0x02
+#define LP5569_INTERNAL_CLK 0x01
+
+#define LP5569_EN_LEDTEST 0x80
+#define LP5569_LEDTEST_DONE 0x80
+#define LP5569_RESET 0xFF
+#define LP5569_ADC_SHORTCIRC_LIM 80
+#define LP5569_EXT_CLK_USED 0x08
+#define LP5569_ENG_STATUS_MASK 0x07
+
+#define LP5569_FADER_MAPPING_MASK 0xC0
+#define LP5569_FADER_MAPPING_SHIFT 6
+
+/* Memory Page Selection */
+#define LP5569_PAGE_ENG1 0
+#define LP5569_PAGE_ENG2 1
+#define LP5569_PAGE_ENG3 2
+#define LP5569_PAGE_MUX1 3
+#define LP5569_PAGE_MUX2 4
+#define LP5569_PAGE_MUX3 5
+
+/* Program Memory Operations */
+#define LP5569_MODE_ENG1_M 0x30 /* Operation Mode Register */
+#define LP5569_MODE_ENG2_M 0x0C
+#define LP5569_MODE_ENG3_M 0x03
+#define LP5569_LOAD_ENG1 0x10
+#define LP5569_LOAD_ENG2 0x04
+#define LP5569_LOAD_ENG3 0x01
+
+#define LP5569_ENG1_IS_LOADING(mode) \
+ ((mode & LP5569_MODE_ENG1_M) == LP5569_LOAD_ENG1)
+#define LP5569_ENG2_IS_LOADING(mode) \
+ ((mode & LP5569_MODE_ENG2_M) == LP5569_LOAD_ENG2)
+#define LP5569_ENG3_IS_LOADING(mode) \
+ ((mode & LP5569_MODE_ENG3_M) == LP5569_LOAD_ENG3)
+
+#define LP5569_EXEC_ENG1_M 0x30 /* Enable Register */
+#define LP5569_EXEC_ENG2_M 0x0C
+#define LP5569_EXEC_ENG3_M 0x03
+#define LP5569_EXEC_M 0x3F
+#define LP5569_RUN_ENG1 0x20
+#define LP5569_RUN_ENG2 0x08
+#define LP5569_RUN_ENG3 0x02
+
+#define LED_ACTIVE(mux, led) (!!(mux & (0x0001 << led)))
+
+enum lp5569_chip_id {
+ LP5569,
+};
+#if 0
+static int lp5569_init_program_engine(struct lp55xx_chip *chip);
+#endif
+static inline void lp5569_wait_opmode_done(void)
+{
+ usleep_range(1000, 2000);
+}
+
+static void lp5569_set_led_current(struct lp55xx_led *led, u8 led_current)
+{
+ led->led_current = led_current;
+ lp55xx_write(led->chip, LP5569_REG_LED_CURRENT_BASE + led->chan_nr,
+ led_current);
+}
+
+static int lp5569_post_init_device(struct lp55xx_chip *chip)
+{
+ int ret;
+
+ /* MISC.int_clk_en bit is STATIC and should only be changed when CONFIG.CHIP_EN = 0 */
+ /* Set internal clock here */
+ ret = lp55xx_write(chip, LP5569_REG_CONFIG, LP5569_INTERNAL_CLK);
+
+ /* then enable en_bit */
+ ret = lp55xx_write(chip, LP5569_REG_ENABLE, LP5569_ENABLE);
+ if (ret)
+ return ret;
+
+ /* Chip startup time is 500 us, 1 - 2 ms gives some margin */
+ usleep_range(1000, 2000);
+
+ ret = lp55xx_write(chip, LP5569_REG_CONFIG,
+ LP5569_AUTO_INC | LP5569_PWR_SAVE |
+ LP5569_CP_AUTO | LP5569_INTERNAL_CLK |
+ LP5569_PWM_PWR_SAVE);
+ if (ret)
+ return ret;
+
+#if 0
+ /* turn on all leds */
+ ret = lp55xx_write(chip, LP5569_REG_ENABLE_LEDS_MSB, 0x01);
+ if (ret)
+ return ret;
+
+ ret = lp55xx_write(chip, LP5569_REG_ENABLE_LEDS_LSB, 0xff);
+ if (ret)
+ return ret;
+ return lp5569_init_program_engine(chip);
+#else
+ return 0;
+#endif
+}
+
+static void lp5569_load_engine(struct lp55xx_chip *chip)
+{
+ enum lp55xx_engine_index idx = chip->engine_idx;
+ u8 mask[] = {
+ [LP55XX_ENGINE_1] = LP5569_MODE_ENG1_M,
+ [LP55XX_ENGINE_2] = LP5569_MODE_ENG2_M,
+ [LP55XX_ENGINE_3] = LP5569_MODE_ENG3_M,
+ };
+
+ u8 val[] = {
+ [LP55XX_ENGINE_1] = LP5569_LOAD_ENG1,
+ [LP55XX_ENGINE_2] = LP5569_LOAD_ENG2,
+ [LP55XX_ENGINE_3] = LP5569_LOAD_ENG3,
+ };
+
+ lp55xx_update_bits(chip, LP5569_REG_OP_MODE, mask[idx], val[idx]);
+
+ lp5569_wait_opmode_done();
+}
+
+static void lp5569_load_engine_and_select_page(struct lp55xx_chip *chip)
+{
+ enum lp55xx_engine_index idx = chip->engine_idx;
+ u8 page_sel[] = {
+ [LP55XX_ENGINE_1] = LP5569_PAGE_ENG1,
+ [LP55XX_ENGINE_2] = LP5569_PAGE_ENG2,
+ [LP55XX_ENGINE_3] = LP5569_PAGE_ENG3,
+ };
+
+ lp5569_load_engine(chip);
+
+ lp55xx_write(chip, LP5569_REG_PROG_PAGE_SEL, page_sel[idx]);
+}
+
+static void lp5569_stop_all_engines(struct lp55xx_chip *chip)
+{
+ lp55xx_write(chip, LP5569_REG_OP_MODE, 0);
+ lp5569_wait_opmode_done();
+}
+
+static void lp5569_stop_engine(struct lp55xx_chip *chip)
+{
+ enum lp55xx_engine_index idx = chip->engine_idx;
+ u8 mask[] = {
+ [LP55XX_ENGINE_1] = LP5569_MODE_ENG1_M,
+ [LP55XX_ENGINE_2] = LP5569_MODE_ENG2_M,
+ [LP55XX_ENGINE_3] = LP5569_MODE_ENG3_M,
+ };
+
+ lp55xx_update_bits(chip, LP5569_REG_OP_MODE, mask[idx], 0);
+
+ lp5569_wait_opmode_done();
+}
+
+static void lp5569_turn_off_channels(struct lp55xx_chip *chip)
+{
+ int i;
+
+ for (i = 0; i < LP5569_MAX_LEDS; i++)
+ lp55xx_write(chip, LP5569_REG_LED_PWM_BASE + i, 0);
+}
+
+static void lp5569_run_engine(struct lp55xx_chip *chip, bool start)
+{
+ int ret;
+ u8 mode;
+ u8 exec;
+
+ /* stop engine */
+ if (!start) {
+ lp5569_stop_engine(chip);
+ lp5569_turn_off_channels(chip);
+ return;
+ }
+
+ /*
+ * To run the engine,
+ * operation mode and enable register should updated at the same time
+ */
+
+ ret = lp55xx_read(chip, LP5569_REG_OP_MODE, &mode);
+ if (ret)
+ return;
+
+ ret = lp55xx_read(chip, LP5569_REG_ENABLE, &exec);
+ if (ret)
+ return;
+
+ /* change operation mode to RUN only when each engine is loading */
+ if (LP5569_ENG1_IS_LOADING(mode)) {
+ mode = (mode & ~LP5569_MODE_ENG1_M) | LP5569_RUN_ENG1;
+ exec = (exec & ~LP5569_EXEC_ENG1_M) | LP5569_RUN_ENG1;
+ }
+
+ if (LP5569_ENG2_IS_LOADING(mode)) {
+ mode = (mode & ~LP5569_MODE_ENG2_M) | LP5569_RUN_ENG2;
+ exec = (exec & ~LP5569_EXEC_ENG2_M) | LP5569_RUN_ENG2;
+ }
+
+ if (LP5569_ENG3_IS_LOADING(mode)) {
+ mode = (mode & ~LP5569_MODE_ENG3_M) | LP5569_RUN_ENG3;
+ exec = (exec & ~LP5569_EXEC_ENG3_M) | LP5569_RUN_ENG3;
+ }
+
+ lp55xx_write(chip, LP5569_REG_OP_MODE, mode);
+ lp5569_wait_opmode_done();
+
+ lp55xx_update_bits(chip, LP5569_REG_ENABLE, LP5569_EXEC_M, exec);
+}
+#if 0
+static int lp5569_init_program_engine(struct lp55xx_chip *chip)
+{
+ int i;
+ int j;
+ int ret;
+ u8 status;
+ /* one pattern per engine setting LED MUX start and stop addresses */
+ static const u8 pattern[][LP5569_PROGRAM_LENGTH] = {
+ { 0x9c, 0x30, 0x9c, 0xb0, 0x9d, 0x80, 0xd8, 0x00, 0},
+ { 0x9c, 0x40, 0x9c, 0xc0, 0x9d, 0x80, 0xd8, 0x00, 0},
+ { 0x9c, 0x50, 0x9c, 0xd0, 0x9d, 0x80, 0xd8, 0x00, 0},
+ };
+
+ /* hardcode 32 bytes of memory for each engine from program memory */
+ ret = lp55xx_write(chip, LP5569_REG_CH1_PROG_START, 0x00);
+ if (ret)
+ return ret;
+
+ ret = lp55xx_write(chip, LP5569_REG_CH2_PROG_START, 0x10);
+ if (ret)
+ return ret;
+
+ ret = lp55xx_write(chip, LP5569_REG_CH3_PROG_START, 0x20);
+ if (ret)
+ return ret;
+
+ /* write LED MUX address space for each engine */
+ for (i = LP55XX_ENGINE_1; i <= LP55XX_ENGINE_3; i++) {
+ chip->engine_idx = i;
+ lp5569_load_engine_and_select_page(chip);
+
+ for (j = 0; j < LP5569_PROGRAM_LENGTH; j++) {
+ ret = lp55xx_write(chip, LP5569_REG_PROG_MEM + j,
+ pattern[i - 1][j]);
+ if (ret)
+ goto out;
+ }
+ }
+
+ lp5569_run_engine(chip, true);
+
+ /* Let the programs run for couple of ms and check the engine status */
+ usleep_range(3000, 6000);
+ lp55xx_read(chip, LP5569_REG_STATUS, &status);
+ status &= LP5569_ENG_STATUS_MASK;
+
+ if (status != LP5569_ENG_STATUS_MASK) {
+ dev_err(&chip->cl->dev,
+ "could not configure LED engine, status = 0x%.2x\n",
+ status);
+ ret = -1;
+ }
+
+out:
+ lp5569_stop_all_engines(chip);
+ return ret;
+}
+#endif
+static int lp5569_update_program_memory(struct lp55xx_chip *chip,
+ const u8 *data, size_t size)
+{
+ u8 pattern[LP5569_PROGRAM_LENGTH] = {0};
+ unsigned cmd;
+ char c[3];
+ int nrchars;
+ int ret;
+ int offset = 0;
+ int i = 0;
+
+ while ((offset < size - 1) && (i < LP5569_PROGRAM_LENGTH)) {
+ /* separate sscanfs because length is working only for %s */
+ ret = sscanf(data + offset, "%2s%n ", c, &nrchars);
+ if (ret != 1)
+ goto err;
+
+ ret = sscanf(c, "%2x", &cmd);
+ if (ret != 1)
+ goto err;
+
+ pattern[i] = (u8)cmd;
+ offset += nrchars;
+ i++;
+ }
+
+ /* Each instruction is 16bit long. Check that length is even */
+ if (i % 2)
+ goto err;
+
+ for (i = 0; i < LP5569_PROGRAM_LENGTH; i++) {
+ ret = lp55xx_write(chip, LP5569_REG_PROG_MEM + i, pattern[i]);
+ if (ret)
+ return -EINVAL;
+ }
+
+ return size;
+
+err:
+ dev_err(&chip->cl->dev, "wrong pattern format\n");
+ return -EINVAL;
+}
+
+static void lp5569_firmware_loaded(struct lp55xx_chip *chip)
+{
+ const struct firmware *fw = chip->fw;
+
+ if (fw->size > LP5569_PROGRAM_LENGTH) {
+ dev_err(&chip->cl->dev, "firmware data size overflow: %zu\n",
+ fw->size);
+ return;
+ }
+
+ /*
+ * Program momery sequence
+ * 1) set engine mode to "LOAD"
+ * 2) write firmware data into program memory
+ */
+
+ lp5569_load_engine_and_select_page(chip);
+ lp5569_update_program_memory(chip, fw->data, fw->size);
+}
+
+static ssize_t show_engine_mode(struct device *dev,
+ struct device_attribute *attr,
+ char *buf, int nr)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
+ struct lp55xx_chip *chip = led->chip;
+ enum lp55xx_engine_mode mode = chip->engines[nr - 1].mode;
+
+ switch (mode) {
+ case LP55XX_ENGINE_RUN:
+ return sprintf(buf, "run\n");
+ case LP55XX_ENGINE_LOAD:
+ return sprintf(buf, "load\n");
+ case LP55XX_ENGINE_DISABLED:
+ default:
+ return sprintf(buf, "disabled\n");
+ }
+}
+show_mode(1)
+show_mode(2)
+show_mode(3)
+
+static ssize_t store_engine_mode(struct device *dev,
+ struct device_attribute *attr,
+ const char *buf, size_t len, int nr)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
+ struct lp55xx_chip *chip = led->chip;
+ struct lp55xx_engine *engine = &chip->engines[nr - 1];
+
+ mutex_lock(&chip->lock);
+
+ chip->engine_idx = nr;
+
+ if (!strncmp(buf, "run", 3)) {
+ lp5569_run_engine(chip, true);
+ engine->mode = LP55XX_ENGINE_RUN;
+ } else if (!strncmp(buf, "load", 4)) {
+ lp5569_stop_engine(chip);
+ lp5569_load_engine(chip);
+ engine->mode = LP55XX_ENGINE_LOAD;
+ } else if (!strncmp(buf, "disabled", 8)) {
+ lp5569_stop_engine(chip);
+ engine->mode = LP55XX_ENGINE_DISABLED;
+ }
+
+ mutex_unlock(&chip->lock);
+
+ return len;
+}
+store_mode(1)
+store_mode(2)
+store_mode(3)
+
+static int lp5569_mux_parse(const char *buf, u16 *mux, size_t len)
+{
+ u16 tmp_mux = 0;
+ int i;
+
+ len = min_t(int, len, LP5569_MAX_LEDS);
+
+ for (i = 0; i < len; i++) {
+ switch (buf[i]) {
+ case '1':
+ tmp_mux |= (1 << i);
+ break;
+ case '0':
+ break;
+ case '\n':
+ i = len;
+ break;
+ default:
+ return -1;
+ }
+ }
+ *mux = tmp_mux;
+
+ return 0;
+}
+
+static void lp5569_mux_to_array(u16 led_mux, char *array)
+{
+ int i, pos = 0;
+ for (i = 0; i < LP5569_MAX_LEDS; i++)
+ pos += sprintf(array + pos, "%x", LED_ACTIVE(led_mux, i));
+
+ array[pos] = '\0';
+}
+
+static ssize_t show_engine_leds(struct device *dev,
+ struct device_attribute *attr,
+ char *buf, int nr)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
+ struct lp55xx_chip *chip = led->chip;
+ char mux[LP5569_MAX_LEDS + 1];
+
+ lp5569_mux_to_array(chip->engines[nr - 1].led_mux, mux);
+
+ return sprintf(buf, "%s\n", mux);
+}
+show_leds(1)
+show_leds(2)
+show_leds(3)
+
+static int lp5569_load_mux(struct lp55xx_chip *chip, u16 mux, int nr)
+{
+ struct lp55xx_engine *engine = &chip->engines[nr - 1];
+ int ret;
+ u8 mux_page[] = {
+ [LP55XX_ENGINE_1] = LP5569_PAGE_MUX1,
+ [LP55XX_ENGINE_2] = LP5569_PAGE_MUX2,
+ [LP55XX_ENGINE_3] = LP5569_PAGE_MUX3,
+ };
+
+ lp5569_load_engine(chip);
+
+ ret = lp55xx_write(chip, LP5569_REG_PROG_PAGE_SEL, mux_page[nr]);
+ if (ret)
+ return ret;
+
+ ret = lp55xx_write(chip, LP5569_REG_PROG_MEM , (u8)(mux >> 8));
+ if (ret)
+ return ret;
+
+ ret = lp55xx_write(chip, LP5569_REG_PROG_MEM + 1, (u8)(mux));
+ if (ret)
+ return ret;
+
+ engine->led_mux = mux;
+ return 0;
+}
+
+static ssize_t store_engine_leds(struct device *dev,
+ struct device_attribute *attr,
+ const char *buf, size_t len, int nr)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
+ struct lp55xx_chip *chip = led->chip;
+ struct lp55xx_engine *engine = &chip->engines[nr - 1];
+ u16 mux = 0;
+ ssize_t ret;
+
+ if (lp5569_mux_parse(buf, &mux, len))
+ return -EINVAL;
+
+ mutex_lock(&chip->lock);
+
+ chip->engine_idx = nr;
+ ret = -EINVAL;
+
+ if (engine->mode != LP55XX_ENGINE_LOAD)
+ goto leave;
+
+ if (lp5569_load_mux(chip, mux, nr))
+ goto leave;
+
+ ret = len;
+leave:
+ mutex_unlock(&chip->lock);
+ return ret;
+}
+store_leds(1)
+store_leds(2)
+store_leds(3)
+
+static ssize_t store_engine_load(struct device *dev,
+ struct device_attribute *attr,
+ const char *buf, size_t len, int nr)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
+ struct lp55xx_chip *chip = led->chip;
+ int ret;
+
+ mutex_lock(&chip->lock);
+
+ chip->engine_idx = nr;
+ lp5569_load_engine_and_select_page(chip);
+ ret = lp5569_update_program_memory(chip, buf, len);
+
+ mutex_unlock(&chip->lock);
+
+ return ret;
+}
+store_load(1)
+store_load(2)
+store_load(3)
+
+static ssize_t lp5569_selftest(struct device *dev,
+ struct device_attribute *attr,
+ char *buf)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
+ struct lp55xx_chip *chip = led->chip;
+ struct lp55xx_platform_data *pdata = chip->pdata;
+ int i, ret, pos = 0;
+ u8 status, adc, vdd;
+
+ mutex_lock(&chip->lock);
+
+ ret = lp55xx_read(chip, LP5569_REG_STATUS, &status);
+ if (ret < 0)
+ goto fail;
+
+ /* Check that ext clock is really in use if requested */
+ if (pdata->clock_mode == LP55XX_CLOCK_EXT) {
+ if ((status & LP5569_EXT_CLK_USED) == 0)
+ goto fail;
+ }
+
+ /* Measure VDD (i.e. VBAT) first (channel 16 corresponds to VDD) */
+ lp55xx_write(chip, LP5569_REG_LED_TEST_CTRL, LP5569_EN_LEDTEST | 16);
+ usleep_range(3000, 6000); /* ADC conversion time is typically 2.7 ms */
+ ret = lp55xx_read(chip, LP5569_REG_STATUS, &status);
+ if (ret < 0)
+ goto fail;
+
+ if (!(status & LP5569_LEDTEST_DONE))
+ usleep_range(3000, 6000); /* Was not ready. Wait little bit */
+
+ ret = lp55xx_read(chip, LP5569_REG_LED_TEST_ADC, &vdd);
+ if (ret < 0)
+ goto fail;
+
+ vdd--; /* There may be some fluctuation in measurement */
+
+ for (i = 0; i < LP5569_MAX_LEDS; i++) {
+ /* Skip non-existing channels */
+ if (pdata->led_config[i].led_current == 0)
+ continue;
+
+ /* Set default current */
+ lp55xx_write(chip, LP5569_REG_LED_CURRENT_BASE + i,
+ pdata->led_config[i].led_current);
+
+ lp55xx_write(chip, LP5569_REG_LED_PWM_BASE + i, 0xff);
+ /* let current stabilize 2 - 4ms before measurements start */
+ usleep_range(2000, 4000);
+ lp55xx_write(chip, LP5569_REG_LED_TEST_CTRL,
+ LP5569_EN_LEDTEST | i);
+ /* ADC conversion time is 2.7 ms typically */
+ usleep_range(3000, 6000);
+ ret = lp55xx_read(chip, LP5569_REG_STATUS, &status);
+ if (ret < 0)
+ goto fail;
+
+ if (!(status & LP5569_LEDTEST_DONE))
+ usleep_range(3000, 6000);/* Was not ready. Wait. */
+
+ ret = lp55xx_read(chip, LP5569_REG_LED_TEST_ADC, &adc);
+ if (ret < 0)
+ goto fail;
+
+ if (adc >= vdd || adc < LP5569_ADC_SHORTCIRC_LIM)
+ pos += sprintf(buf + pos, "LED %d FAIL\n", i);
+
+ lp55xx_write(chip, LP5569_REG_LED_PWM_BASE + i, 0x00);
+
+ /* Restore current */
+ lp55xx_write(chip, LP5569_REG_LED_CURRENT_BASE + i,
+ led->led_current);
+ led++;
+ }
+ if (pos == 0)
+ pos = sprintf(buf, "OK\n");
+ goto release_lock;
+fail:
+ pos = sprintf(buf, "FAIL\n");
+
+release_lock:
+ mutex_unlock(&chip->lock);
+
+ return pos;
+}
+
+#define show_fader(nr) \
+static ssize_t show_master_fader##nr(struct device *dev, \
+ struct device_attribute *attr, \
+ char *buf) \
+{ \
+ return show_master_fader(dev, attr, buf, nr); \
+}
+
+#define store_fader(nr) \
+static ssize_t store_master_fader##nr(struct device *dev, \
+ struct device_attribute *attr, \
+ const char *buf, size_t len) \
+{ \
+ return store_master_fader(dev, attr, buf, len, nr); \
+}
+
+static ssize_t show_master_fader(struct device *dev,
+ struct device_attribute *attr,
+ char *buf, int nr)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
+ struct lp55xx_chip *chip = led->chip;
+ int ret;
+ u8 val;
+
+ mutex_lock(&chip->lock);
+ ret = lp55xx_read(chip, LP5569_REG_MASTER_FADER_BASE + nr - 1, &val);
+ mutex_unlock(&chip->lock);
+
+ if (ret == 0)
+ ret = sprintf(buf, "%u\n", val);
+
+ return ret;
+}
+show_fader(1)
+show_fader(2)
+show_fader(3)
+
+static ssize_t store_master_fader(struct device *dev,
+ struct device_attribute *attr,
+ const char *buf, size_t len, int nr)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
+ struct lp55xx_chip *chip = led->chip;
+ int ret;
+ unsigned long val;
+
+ if (kstrtoul(buf, 0, &val))
+ return -EINVAL;
+
+ if (val > 0xff)
+ return -EINVAL;
+
+ mutex_lock(&chip->lock);
+ ret = lp55xx_write(chip, LP5569_REG_MASTER_FADER_BASE + nr - 1,
+ (u8)val);
+ mutex_unlock(&chip->lock);
+
+ if (ret == 0)
+ ret = len;
+
+ return ret;
+}
+store_fader(1)
+store_fader(2)
+store_fader(3)
+
+static ssize_t show_master_fader_leds(struct device *dev,
+ struct device_attribute *attr,
+ char *buf)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
+ struct lp55xx_chip *chip = led->chip;
+ int i, ret, pos = 0;
+ u8 val;
+
+ mutex_lock(&chip->lock);
+
+ for (i = 0; i < LP5569_MAX_LEDS; i++) {
+ ret = lp55xx_read(chip, LP5569_REG_LED_CTRL_BASE + i, &val);
+ if (ret)
+ goto leave;
+
+ val = (val & LP5569_FADER_MAPPING_MASK)
+ >> LP5569_FADER_MAPPING_SHIFT;
+ if (val > 3) {
+ ret = -EINVAL;
+ goto leave;
+ }
+ buf[pos++] = val + '0';
+ }
+ buf[pos++] = '\n';
+ ret = pos;
+leave:
+ mutex_unlock(&chip->lock);
+ return ret;
+}
+
+static ssize_t store_master_fader_leds(struct device *dev,
+ struct device_attribute *attr,
+ const char *buf, size_t len)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
+ struct lp55xx_chip *chip = led->chip;
+ int i, n, ret;
+ u8 val;
+
+ n = min_t(int, len, LP5569_MAX_LEDS);
+
+ mutex_lock(&chip->lock);
+
+ for (i = 0; i < n; i++) {
+ if (buf[i] >= '0' && buf[i] <= '3') {
+ val = (buf[i] - '0') << LP5569_FADER_MAPPING_SHIFT;
+ ret = lp55xx_update_bits(chip,
+ LP5569_REG_LED_CTRL_BASE + i,
+ LP5569_FADER_MAPPING_MASK,
+ val);
+ if (ret)
+ goto leave;
+ } else {
+ ret = -EINVAL;
+ goto leave;
+ }
+ }
+ ret = len;
+leave:
+ mutex_unlock(&chip->lock);
+ return ret;
+}
+
+static int lp5569_led_brightness(struct lp55xx_led *led)
+{
+ struct lp55xx_chip *chip = led->chip;
+ int ret;
+
+ mutex_lock(&chip->lock);
+ ret = lp55xx_write(chip, LP5569_REG_LED_PWM_BASE + led->chan_nr,
+ led->brightness);
+ mutex_unlock(&chip->lock);
+ return ret;
+}
+
+static LP55XX_DEV_ATTR_RW(engine1_mode, show_engine1_mode, store_engine1_mode);
+static LP55XX_DEV_ATTR_RW(engine2_mode, show_engine2_mode, store_engine2_mode);
+static LP55XX_DEV_ATTR_RW(engine3_mode, show_engine3_mode, store_engine3_mode);
+static LP55XX_DEV_ATTR_RW(engine1_leds, show_engine1_leds, store_engine1_leds);
+static LP55XX_DEV_ATTR_RW(engine2_leds, show_engine2_leds, store_engine2_leds);
+static LP55XX_DEV_ATTR_RW(engine3_leds, show_engine3_leds, store_engine3_leds);
+static LP55XX_DEV_ATTR_WO(engine1_load, store_engine1_load);
+static LP55XX_DEV_ATTR_WO(engine2_load, store_engine2_load);
+static LP55XX_DEV_ATTR_WO(engine3_load, store_engine3_load);
+static LP55XX_DEV_ATTR_RO(selftest, lp5569_selftest);
+static LP55XX_DEV_ATTR_RW(master_fader1, show_master_fader1,
+ store_master_fader1);
+static LP55XX_DEV_ATTR_RW(master_fader2, show_master_fader2,
+ store_master_fader2);
+static LP55XX_DEV_ATTR_RW(master_fader3, show_master_fader3,
+ store_master_fader3);
+static LP55XX_DEV_ATTR_RW(master_fader_leds, show_master_fader_leds,
+ store_master_fader_leds);
+
+static struct attribute *lp5569_attributes[] = {
+ &dev_attr_engine1_mode.attr,
+ &dev_attr_engine2_mode.attr,
+ &dev_attr_engine3_mode.attr,
+ &dev_attr_engine1_load.attr,
+ &dev_attr_engine2_load.attr,
+ &dev_attr_engine3_load.attr,
+ &dev_attr_engine1_leds.attr,
+ &dev_attr_engine2_leds.attr,
+ &dev_attr_engine3_leds.attr,
+ &dev_attr_selftest.attr,
+ &dev_attr_master_fader1.attr,
+ &dev_attr_master_fader2.attr,
+ &dev_attr_master_fader3.attr,
+ &dev_attr_master_fader_leds.attr,
+ NULL,
+};
+
+static const struct attribute_group lp5569_group = {
+ .attrs = lp5569_attributes,
+};
+
+/* Chip specific configurations */
+static struct lp55xx_device_config lp5569_cfg = {
+ .reset = {
+ .addr = LP5569_REG_RESET,
+ .val = LP5569_RESET,
+ },
+ .enable = {
+ .addr = LP5569_REG_ENABLE,
+ .val = LP5569_ENABLE,
+ },
+ .max_channel = LP5569_MAX_LEDS,
+ .post_init_device = lp5569_post_init_device,
+ .brightness_fn = lp5569_led_brightness,
+ .set_led_current = lp5569_set_led_current,
+ .firmware_cb = lp5569_firmware_loaded,
+ .run_engine = lp5569_run_engine,
+ .dev_attr_group = &lp5569_group,
+};
+
+static int lp5569_probe(struct i2c_client *client,
+ const struct i2c_device_id *id)
+{
+ int ret;
+ struct lp55xx_chip *chip;
+ struct lp55xx_led *led;
+ struct lp55xx_platform_data *pdata = dev_get_platdata(&client->dev);
+ struct device_node *np = client->dev.of_node;
+
+ if (!pdata) {
+ if (np) {
+ pdata = lp55xx_of_populate_pdata(&client->dev, np);
+ if (IS_ERR(pdata))
+ return PTR_ERR(pdata);
+ } else {
+ dev_err(&client->dev, "no platform data\n");
+ return -EINVAL;
+ }
+ }
+
+ chip = devm_kzalloc(&client->dev, sizeof(*chip), GFP_KERNEL);
+ if (!chip)
+ return -ENOMEM;
+
+ led = devm_kzalloc(&client->dev,
+ sizeof(*led) * pdata->num_channels, GFP_KERNEL);
+ if (!led)
+ return -ENOMEM;
+
+ chip->cl = client;
+ chip->pdata = pdata;
+ chip->cfg = &lp5569_cfg;
+
+ mutex_init(&chip->lock);
+
+ i2c_set_clientdata(client, led);
+
+ ret = lp55xx_init_device(chip);
+ if (ret)
+ goto err_init;
+
+ dev_info(&client->dev, "%s Programmable led chip found\n", id->name);
+
+ ret = lp55xx_register_leds(led, chip);
+ if (ret)
+ goto err_register_leds;
+
+ ret = lp55xx_register_sysfs(chip);
+ if (ret) {
+ dev_err(&client->dev, "registering sysfs failed\n");
+ goto err_register_sysfs;
+ }
+
+ return 0;
+
+err_register_sysfs:
+ lp55xx_unregister_leds(led, chip);
+err_register_leds:
+ lp55xx_deinit_device(chip);
+err_init:
+ return ret;
+}
+
+static int lp5569_remove(struct i2c_client *client)
+{
+ struct lp55xx_led *led = i2c_get_clientdata(client);
+ struct lp55xx_chip *chip = led->chip;
+
+ lp5569_stop_all_engines(chip);
+ lp55xx_unregister_sysfs(chip);
+ lp55xx_unregister_leds(led, chip);
+ lp55xx_deinit_device(chip);
+
+ return 0;
+}
+
+static const struct i2c_device_id lp5569_id[] = {
+ { "lp5569", LP5569 },
+ { }
+};
+
+MODULE_DEVICE_TABLE(i2c, lp5569_id);
+
+#ifdef CONFIG_OF
+static const struct of_device_id of_lp5569_leds_match[] = {
+ { .compatible = "national,lp5569", },
+ { .compatible = "ti,lp5569", },
+ {},
+};
+
+MODULE_DEVICE_TABLE(of, of_lp5569_leds_match);
+#endif
+
+static struct i2c_driver lp5569_driver = {
+ .driver = {
+ .name = "lp5569x",
+ .of_match_table = of_match_ptr(of_lp5569_leds_match),
+ },
+ .probe = lp5569_probe,
+ .remove = lp5569_remove,
+ .id_table = lp5569_id,
+};
+
+module_i2c_driver(lp5569_driver);
+
+MODULE_AUTHOR("Mathias Nyman <mathias.nyman@nokia.com>");
+MODULE_AUTHOR("Milo Kim <milo.kim@ti.com>");
+MODULE_AUTHOR("Woonyong Yun <wyyun@humaxdigital.com>");
+MODULE_DESCRIPTION("LP5569 LED engine");
+MODULE_LICENSE("GPL");
Here is my works till now.
After review my works and fix the engine loading logic. It would be best!
Thanks & Regards,
WY, Yun