Other Parts Discussed in Thread: BQ35100
Good afternoon.
I am attempting to implement the BQ34Z100-G1 (using the evaluation module) to gauge the SOC of two series CR123 batteries.
These batteries are not rechargeable, meaning when they are "dead" they are replaced with a fresh pair of batteries.
So I believe I have set the chemistry properly and all of the flash parameters, but I am unsure if I will ever successfully complete a learning cycle...
In most documentation I have read, you are required to charge the battery pack which is part of the learning cycle, however when I get to that point I simply replace
the batteries. In doing so it powers down the evaluation module which then comes up again with the new batteries.
Will I ever complete a learning cycle this way, or am I spinning my wheels? Secondly are there any other flash parameters that need to be set to allow for this?
Thank you for your time.