This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3: bq27510-G3 / Use NCR18650BF (ID:2050) battery with 4.1V charging and 3.0V EDV

Part Number: BQ27510-G3

Hi,

The customer consider to use bq27510-G3 with NCR18650BF (ID:2050) battery and we know that this battery was characterized with 4.2V charging voltage and 2.5V EDV. But now they'd like to use this battery with 4.1V charging and 3.0V EDV in their system. Then please let me ask following question.

  1. At learning cycle, should we set charging voltage to 4.2V and EDV to 2.5V for this battery?
  2. If the answer for #1 is yes, can we achieve correct accuracy with golden image at 4.1V charging and 3.0V EDV usage?

Best Regards,

Satoshi / Japan Disty